New ProductNewsPress ReleasesPress Releases

New C-more Micro Operator Interface Panel

AutomationDirect’s new EA3-T6CL 6” C-more Micro touch panel has a 5.7-inch TFT LCD 320 x 240 dot display and a palette of 32K colors for customizing objects, screen backgrounds and displaying bitmap graphics. Powered from a Class 2, 12-24 VDC power supply, it features three communications ports (USB programming, RJ12 and DB15) and five user-defined function keys,EA3 C-More Micro Touch Panel each key with a user-defined red LED indicator.

In landscape orientation, the panel can display up to 40 lines by 80 characters of static text or up to 40 lines by 40 characters of dynamic text with embedded variables and phrases mixed with graphics; portrait orientation can display 53 lines by 60 characters of static text or 40 lines by 40 characters of dynamic text. The 6” C-more Micro TFT panel is priced at $299.00 and is backed with a two-year warranty.

Click here for more information.

To read more articles about operator interface, click here.c-more-cta-600x190

About AutomationDirect:

In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.

*Prices as of November 4, 2015. Check website for most current prices.