Replacing & Sizing AC Motors | White Paper

The decision to replace existing motors with newer premium efficiency motors can be difficult. And, a common mistake made is thinking that buying any new premium efficiency motor will deliver optimal efficiency. This paper discusses how to determine whether to rewind or replace a motor, and how to find the right motor size for the application.Replacing and Sizing an AC Motor

This new White Paper explains the three basic standards of motor efficiency: pre-EPAct, EPAct, and Premium Efficiency (also known as NEMA Premium). It also contains considerations for determining when rewinding the motor’s coils may be the better option over replacing the motor. Likewise, considerations are given to determine when motor replacement is the better option.

This White Paper also provides important factors when selecting the proper size replacement AC motor. A too-frequent problem in today’s industrial applications is the use of oversized motors. The paper explains that this issue is easily addressed with more precise up-front engineering, such as conducting a motor survey to correctly size a replacement motor.

The Important Considerations for Replacing and Sizing AC Motors White Paper can be downloaded as a PDF here.

 
Download free AC Motor White Paper now
 

About AutomationDirect:

In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency and the majority of their products are stocked for same-day shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.

 

 
© 2015 Library at AutomationDirect.com
Owned and Operated by AutomationDirect.com