NewsPress ReleasesPress Releases

STEGO Filter Fan Plus enclosure cooling fans

AutomationDirect has added the new STEGO Filter Fan Plus series of enclosure fans to its enclosure thermal management devices lineup.

Filter fans provide economical cooling options for electrical/electronic enclosures. The STEGO Filter Fan Plus series uses a new air flap design for the air outlet. The air flaps have less resistance to airflow than an exhaust filter, which allows the Filter Fan Plus system to achieve higher airflow while still preventing the ingress of contaminants.

Filter Fan Plus enclosure fans are offered in five cutout sizes ranging from 3.62 x 3.62 inches to 11.46 x 11.46 inches with 120, 230VAC and 12, 24, 48VDC models available.

Two airflow system styles are available, with flow ranges from 7.4 CFM to 243 CFM. The FPI system has an intake fan with filter and an exhaust grille with air flaps, while the FPO system uses an exhaust fan with air flaps and an intake grille with filter.

All Filter Fan Plus fans and grilles feature a true “no screw” mounting system using four 6-position ratchets to firmly mount the fan. Ratchets can be released should the fan need to be removed. Screws can still be used for mounting if desired and are provided. A screw drilling template is molded into the housing. Hinged covers on all fans and grilles facilitate quick and easy filter changes.

The STEGO Filter Fan Plus series is IP54 dust and splash waterproof rated and has a UL94V-0 Flammability Rating. Prices start at $60.00.

Learn more by visiting: www.automationdirect.com/enclosure-fans

About AutomationDirect:

In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.

*Prices as of August 9th, 2017. Check website for most current prices