• Home
  • Posts Tagged'Water'

Posts Tagged ‘Water’

ProSense Line Now Includes Float Level Switches

Cumming, GA — January 15, 2014  AutomationDirect’s ProSense line has been extended to include float level switches which provide a low-cost general purpose solution for single point monitoring of liquid levels in a variety of applications. The float switches …

Read more →
 

PLCs Give Wastewater Pumping Stations a Lift – Issue 19, 2011

Flexible, economical PLCs provide automatic failover, backup pump control, and remote lift station monitoring.

The Moccasin Bend Wastewater Treatment Plant (WWTP) is part of the Interceptor Sewer System, which has served Chattanooga, Tennessee, and its surrounding metropolitan areas since it …

Read more →
 

Upgrading Pump Stations with PLCs – Issue 20, 2011

When relays and timer circuits get old, they cause problems. Replacing them with PLCs keeps pumps running smoothly.

One of the most important jobs of a water distribution system is to reliably deliver water to its customers. At our water …

Read more →
 

Evolution of the ChemFreePro® Ion Generator – Issue 16, 2010

In the 1960s, NASA conducted a research program to develop a small lightweight water purifier. The purifier was for use in the Apollo spacecraft, so low power usage and minimal maintenance were a must. The 9-ounce purifier, slightly larger than …

Read more →
 

Dredging Up The…FUTURE – Issue 6, 2006

People around the world are aware of the devastation caused by Hurricane Katrina along the coast of Louisiana, Mississippi, Alabama, and Florida. What started around the southeastern Bahamas on August 23, 2005 as Tropical Depression number 12, quickly became the …

Read more →
 

Ever Wonder How AutomationDirect Customers Are Applying Their Products? – Issue 2, 2004

Check out some of the application stories we’ve collected and you’ll see that AutomationDirect products are used in a wide variety of applications across many different industries. —
Jump to Application Spotlight

D2-250 PLC PID Loops Control Pumps In Residential

Read more →
 
© 2015 Library at AutomationDirect.com
Owned and Operated by AutomationDirect.com