AutomationDirect has expanded its Marathon AC motor line to include lower-cost, high-performance 0.5 to 5 HP Marathon Max+ series AC motors with integrated encoder. The 230/460 VAC Max+ inverter-duty motors are designed to replace 90 and 180 volt Permanent Magnet DC (PMDC) systems,
The following How-to video covers the proper installation for the Dynapar HS35 heavy-duty hollow shaft encoder on a Marathon motor in six easy steps. Before you get started make sure to inspect all the parts and locate all the tools required for this installation. Luckily, AutomationDirect.com has created these Marathon Replacement Encoder Kits to come with…
ApplicationApplication StoriesAutomation NotebookIndustryIssue 6 – 2006Learning ResourcesMachine ControlMotorsNotebook IssueOperator InterfacePackagingPLCProductProgrammable ControlUser SolutionsVariable Speed Drives
System Integrator Slashes Retrofit Price While Adding Value
Box Making Machine Retrofit Project in Ravenna, OH CorrTech, Inc. is an industrial machinery services company that focuses on the corrugated paper and container industry. One of their customers, Smurfit Stone Enterprises in Ravenna, Ohio, recently requested the retrofit of a heavy-duty box-making machine built in the US circa 1970. The S&S ZLR Flexo Folder…