Our Group Motor Protection White Paper explains how the usual way of preventing a small motor from drawing too much current is to install overcurrent protection in the form of a circuit breaker or some other kind of limiter. But installations that employ more than one motor might not want to use this approach. What’s Inside? By using…
Cumming, GA — August 22, 2012 … AutomationDirect’s IronHorse™ general purpose AC motor line now includes stainless steel three-phase motors available in horsepower ranges from 0.33 to 2 hp. Motors are available in speeds of 1800 and 3600 RPM and are electrically reversible. The three-phase industrial duty 56C-frame TEFC motors, priced from $275, feature 304 stainless steel frames…
ApplicationApplication StoriesAutomation NotebookAutomationDirect SpotlightDrivesEducation/DIYEntertainmentHMIIndustryIssue 19 – 2011Learning ResourcesMachine ControlMotorsNotebook IssueOperator InterfacePLCPLC eBookProductProgrammable ControlStudent SpotlightStudent SpotlightVariable Speed Drives
Automated Volleyball Server
Larry May, a student at Southern Polytechnic State University (SPSU), contacted AutomationDirect and outlined his goal of building a volleyball setting and serving machine for his senior design project. Larry is active as a recreational volleyball player and is the father and coach of a competitive high school player. Larry is also a long time…
How many types of DC motors are there? There are several types of DC motors, including shunt, series, compound wound or stabilized shunt, permanent magnet, and brushless DC. The main differences between these types of motors revolve around how the electromagnetic fields are generated. The IronHorse DC motors are Permanent Magnet motors: the magnetic field…
Automation NotebookCompany TopicsIssue 13 – 2009Learning ResourcesNewsNotebook IssueProductProgrammable ControlTech Thread
Online Resources Provide A Wealth Of Information
Visit our primary Web site at www.AutomationDirect.com and take advantage of the information and assistance available to you with the click of a mouse, including obtaining quotes and real-time stock checks. If you are a registered user, you can access additional details such as pending orders, processed orders and invoice history. For even more time savings, check…
+Tech TopicsAutomation NotebookFYIIssue 10 – 2008Learning ResourcesMotorsNotebook IssueProductVariable Speed Drives
Motor Questions Answered
FAQS Question: Can IronHorse™ motors be used with a drive? Answer: IronHorse™ motors can be used with drives, but there are some limitations. Depending on your application, there may be good reasons to step up to an inverter-duty motor in your application. Question: What’s the difference between a General Purpose motor and an Inverter Duty motor? Answer: General…
ApplicationApplication StoriesAutomation NotebookIndustryIssue 6 – 2006Learning ResourcesMachine ControlMotorsNotebook IssueOperator InterfacePackagingPLCProductProgrammable ControlUser SolutionsVariable Speed Drives
System Integrator Slashes Retrofit Price While Adding Value
Box Making Machine Retrofit Project in Ravenna, OH CorrTech, Inc. is an industrial machinery services company that focuses on the corrugated paper and container industry. One of their customers, Smurfit Stone Enterprises in Ravenna, Ohio, recently requested the retrofit of a heavy-duty box-making machine built in the US circa 1970. The S&S ZLR Flexo Folder…
ApplicationAutomation NotebookFeature StoryIssue 2 – 2004Learning ResourcesManufacturingMotorsNotebook IssueProduct
Strides in Motor Technology
When AutomationDirect was looking to provide customers with a high-performance, cost effective drive/motor package to complement their growing line of AC variable speed drives, they turned to Marathon Electric – a well-recognized, well-respected name in the industry. Marathon manufactures a full line of general purpose, inverter-duty, vector-duty and NEMA premium efficiency motors to meet the…
AutomationDirect recently released the custom-built DURApulse™ drives line, and announced a partnership with Marathon Electric® to offer a wide range of Marathon’s vector and inverter-duty motors. These new drives and motors are available up to 100 hp and, when purchased in approved combinations, feature some of the lowest prices in the industry. The new DURApulse™…