ProSense Q&A
+Tech TopicsAutomation NotebookFYIIssue 11 – 2008Learning ResourcesNotebook IssueProcess Sensing & ControlProduct

ProSense Q&A

When selecting a pressure sensor, what factors should I consider? There are three primary considerations when selecting a pressure sensor; pressure values the system will have, temperature of the process material and the compatibility of the sensor with the process fluid. System pressure values – the normal working pressure should be below the maximum range of…
AutomationDirect Offers Pressure Sensors
Issue 11 – 2008NewsNotebook IssuePress Releases

AutomationDirect Offers Pressure Sensors

AutomationDirect has added ProSense™ pressure switches and transmitters to its growing offering of sensor products. ProSense pressure sensors are designed to monitor system pressure in hydraulic and pneumatic applications, while the vacuum sensors provide an accurate readout of increases and decreases in vacuum systems. ProSense sensors are smaller and easier to install than traditional mechanical…