During the summer of 2015, while many Scouts were going to traditional summer camps, a group of Scouts from the Twin Rivers Council in New York spent a week at STEM Camp where they participated in Electronics, Engineering, Surveying, and Programming Merit Badges. The Scouts were thrilled to learn how to program the same PLCs that…
A common function of a control system is detecting the presence of an object. Whether you are detecting the presence of an object passing by on a conveyor, the closure of a gate or the position of a machine part as it goes through its motions, object detection is a staple of the automation industry. There are…
+Tech TopicsAutomation NotebookFYIIssue 13 – 2009Learning ResourcesNotebook IssueProductProgrammable Control
CLICK™ PLC FAQs
Will the CLICK PLC work with my C-more and C-more Micro graphics panels? Yes. Currently the CLICK PLC driver is available in the C-more Micro panel with firmware version 0201001 or later, so native CLICK addresses are available. The CLICK PLC driver for C-more touch panels is currently under development and scheduled to be available soon. You can communicate…