When To Use Multi-function Safety Relays | White Paper

Multi-function safety relays are often the best choice for applications where single-function relays aren’t capable enough and a safety-rated PLC is overkill. This White Paper describes how multi-function safety relays can often improve application costs by replacing multiple basic single-function safety relays.

AutomationDirect announces the release of a new White Paper, “When to Use Multi-Function Safety Relays” that explains how to determine when applications will benefit from multi-function safety relays over other options.multi-function-safety-relays

Many machines and robots require safety circuits to stop all or part of operation in the event of an emergency. Safety circuits are also used to keep all or part of a machine or robot from running while there is human activity in close proximity, either for normal operations or maintenance.

The White Paper describes how one or more multi-function safety relays can often be used to replace many basic single-function safety relays, simplifying installations and saving money. In many cases, multi-function safety relays can be used instead of a safety-rated PLC, resulting in substantial savings while streamlining implementation and maintenance.

This White Paper also explains that machines and robots with just a couple of basic safety inputs, such as an E-stop and one or two door switches or other safety-related inputs, are typically best served by a safety system with one or two single-function safety relays. When a machine has many I/O points, with a high proportion safety-related, a safety-rated PLC is often the best fit. But for a machine or robot in between these two extremes, an easy to configure and inexpensive safety system using multi-function relays may be the preferred choice.

The White Paper is available as a Word document or can be downloaded as a PDF at: www.automationdirect.com/static/press//When-to-use-multi-function-safety-relays-white-paper.pdf

 

About AutomationDirect:

In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor control, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their model and focus on efficiency and the majority of their products are stocked for same-day shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.

 

 
© 2015 Library at AutomationDirect.com
Owned and Operated by AutomationDirect.com