Generators efficiently convert low-grade waste heat from diesel generators into power. Joe Thibedeau, a control systems engineer with ElectraTherm, wrote an article for the November 2019 issue of Power titled Innovative Technology Captures Energy from Waste Heat. Here’s a summary, click on the link above for the full text. Dutch Harbor power plant in the…
+Tech TopicsApplicationApplication StoriesEnergy/UtilitiesHMIIndustryLearning ResourcesMachine ControlManufacturingOperator InterfacePLCProductProgrammable Control
Honing in on Machine Automation
The automation and electrical system on a large, 82-year-old cylinder honing machine was replaced with a variety of AutomationDirect hardware to improve cycle time, safety and quality. Andrew Marks, Maintenance Foreman and Master Electrician at Exline Leasing Inc., wrote an article for the January 2019 issue of Control Design magazine, titled Honing in on Machine…
ApplicationApplication StoriesEnergy/UtilitiesFacilitiesHMIIndustryLearning ResourcesOnline BlogOnline OnlyPLCProcess Control
System Integrator and AutomationDirect partner Affinity Energy Designed, Built and Installed a Research Chamber Temperature Control System
The University of North Carolina (UNC) at Chapel Hill spends almost $1 billion on research annually, ranking eighth among universities in the U.S. However, it was spending too much money and time supporting an existing temperature chamber control system.
ApplicationApplication StoriesEnergy/UtilitiesIndustryLearning ResourcesOnline BlogOnline OnlyOperator InterfacePLCProcess ControlProductProgrammable Control
Automating Hazardous Gas Delivery
When a highly flammable, toxic and corrosive gas delivery system for semiconductor production tools became unreliable, Headway Technologies contracted with system integrator KCC Software for the needed upgrades. KCC Software’s experience and expertise led to the successful replacement of a failing automation system with a new automatic gas control (AGC) system.
+Tech TopicsApplicationCommunicationsData System MonitoringEnergy/UtilitiesIndustryLearning ResourcesOnline OnlyOperator InterfaceProduct
A Quick View of SCADA in Oil and Gas
For quick and secure access to production and process data, a PC-based supervisory control and data acquisition (SCADA) system is often the best solution. Whether upstream, midstream or downstream in the process, data can be collected by the SCADA system using a variety of built-in tools. Once collected from controllers and smart devices, the data…
ApplicationApplication StoriesAutomationDirect SpotlightEducation/DIYEnergy/UtilitiesIndustryPLCProcess ControlProductProgrammable ControlStudent SpotlightUncategorized
Experience is the Best Teacher
Colorado Mountain College’s Applied Engineering Technician Program partnered with AutomationDirect to provide their students with real-world experience using state-of-the-art automation technology. Working with AutomationDirect controllers, the CMC students apply what they’ve learned in the classroom to real equipment used in process control applications. The following excerpt from the CMC campus newsletter explains the opportunities further…
+Tech TopicsApplicationEnergy/UtilitiesIndustryLearning ResourcesMachine ControlOnline OnlyProcess Sensing & ControlProductVariable Speed Drives
Trending Towards Green Machines
When wandering the plant floor, keep an eye out for energy wasting machines. Those running conveyors, rattling pumps and hissing air lines on idle equipment not only raise the decibel level in the plant—they also waste energy. With proper monitoring and analysis, machine energy use can be optimized, and these energy saving measures will also improve…
ApplicationApplication StoriesAutomation NotebookAutomationDirect SpotlightEducation/DIYEnergy/UtilitiesIndustryIssue 30 - 2014Learning ResourcesMachine ControlMotion ControlNotebook IssuePLCPneumaticsProductStudent SpotlightStudent Spotlight
UCONN Student Design Team Automates RFID Tagging
In the aerospace industry, any substance that is foreign to the aircraft engine and could potentially cause damage is known as FOD (foreign object debris). FOD costs the industry 4 billion dollars per year on average. Some of the most common causes of FOD damage are the tools required to build or maintain the engine….
ApplicationApplication StoriesAutomation NotebookAutomationDirect SpotlightDrivesEducation/DIYEnergy/UtilitiesHMIIndustryIssue 29 - 2014Learning ResourcesNotebook IssueOperator InterfacePLCProcess ControlProductProgrammable ControlStudent SpotlightStudent SpotlightVariable Speed Drives
People's Choice for a Cost-Effective and Energy-Efficient Solar-Powered Home
UrbanEden, the University of North Carolina at Charlotte’s entry to the Solar Decathlon 2013, is a concept home consisting of four connected indoor and outdoor spaces that create a unique
ApplicationApplication StoriesAutomation NotebookData System MonitoringEnergy/UtilitiesIndustryIssue 27 – 2013Learning ResourcesNotebook IssuePLCProductProgrammable ControlUser Solutions
Switching to Do-more Saves Time
Almost 14 years ago, I converted the controls in my 80KW hydro electric plant, located in the mountains of western North Carolina, from custom micro-controller cards I developed while at Georgia Tech to the DirectLOGIC DL205 PLC with a D2-260 CPU. In 2013, it was time to make some upgrades to the plant by adding…