Processor Power and Efficiency | White Paper

While energy efficiency is vital for consumer electronics, the industrial automation customer also benefits from chip manufacturers’ perpetual goal to create processors that do more while using less energy. This White Paper explains how consumer electronic microprocessor improvements also provide a catalyst for industrial automation advancements.

processor-power-energy-efficiency-coverSeptember 10, 2014 — AutomationDirect announces the release of a new White Paper, “Processor Power and Energy Efficiency”.

Modern electronic devices, such as smart phones, tablets, etc. can be used to perform a myriad of tasks including messaging, photos, videos, music, alarms, day planners, GPS and more. The same trend of combining what once required several components into one device is also apparent in industrial automation.

The White Paper explains that while energy efficiency is vital for consumer electronics, new powerful chips offer many advantages to the automation world in terms of price, time-to-market, flexibility and reliability.

This is evident in modern PLCs. The integration of more components into microprocessors has eliminated the need for additional external automation components. These components include, but are not limited to, data loggers, ASCII or math co-processors, digital communication cards, proportional-integral-derivative (PID) controllers and more.

This White Paper explains how consolidating functionality into fewer components also creates lower overall costs and power usage for the total system, while providing easier integration and greater reliability.

The White Paper can be downloaded as a PDF at:

www.automationdirect.com/static/press/Processor-power-and-energy-efficiency-white-paper.pdf

free-white-paper-download

 

About AutomationDirect:

In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency and the majority of their products are stocked for same-day shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com

 
© 2015 Library at AutomationDirect.com
Owned and Operated by AutomationDirect.com