NewsPress ReleasesPress Releases

AutomationDirect adds SapiSelco Cable/Wire Ties and Installation Tools

AutomationDirect has added a complete new line of cable and wire ties from the manufacturer SapiSelco. SapiSelco® has been a leader in the manufacture of cable ties for more than 65 years, offering a wide variety of standard and specialty cable ties.

Standard cable ties (starting at $1.00 / 300pcs) are available in natural, black and five colors, have rounded edges to avoid cable damage, and are UL 94: V2 self-extinguishing Nylon rated. Stainless steel tooth Nylon cable ties (from $1.50 / 150pcs) (with added Molybdenum) provide extremely high mechanical strength and optimal resistance to corrosion.

SapiSelco specialty cable ties include UV resistant ties, metal detector readable ties (recommended in the food, pharmaceutical and chemical industry), pushbutton re-openable/reusable ties, buttonhole ties, screw mount tie to attach cable bundles to a support, Nylon marker cable ties with built-in identification tag, and double-headed locking cable ties for more secure fastening.

Starting at $12.50, available SapiSelco cable tie tools include cutting tools, collar fastening tools, and an adjustable cable tie gun installation tool.

Learn more by visiting: www.automationdirect.com/cable-tie

About AutomationDirect:

In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.

*Prices as of August 23rd, 2017. Check website for most current prices