New ProductNewsPress ReleasesPress Releases

Choosing an Industrial Automation Controller – White Paper from AutomationDirect

AutomationDirect announces the release of a new White Paper, “How to choose an Industrial Automation Controller”, which discusses the evaluation of critical factors required in the specification of an automation controller for the industrial environment. The controller selected, such as a PLC or PAC, can control a single station, a machine, a process unit, a whole assembly line or an entire plant.

What’s Inside?

Factors to be considered when choosing a controller include new or existing system automation, environmental issues, I/O locations (local and remote), discrete and analog devices, loop control, specialty features and modules, communication and programming.

This White Paper discusses the number, types and location of I/O; communications requirements among multiple controllers, peripheral devices and enterprise-level systems; memory, scan-time speed and battery backup hardware aspects; software platform and programming methods; and the availability of PID loops, floating-point math, drum sequencing, program interrupts and subroutines.

Whether the system is new or existing often dictates many of the critical factors for selection. If extreme environmental conditions exist, ambient temperature limits can be a critical issue. Actual conditions at the plant floor level or specific codes in force at the facility may demand tougher design considerations.

The “How to choose an Industrial Automation Controller” White Paper can be downloaded here.

About AutomationDirect:

In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.

Editorial Contact:              Tina Gable

Phone:                                678-455-1845

Email:                                tgable@automationdirect.com