December 4, 2024 – AutomationDirect has added high quality Helukabel unshielded “extra hard use” 600V SOOW and 300V SJOOW portable cord. Portable cord (also called service cord) is cable with multiple conductors used for electrical power connections that are not intended to be permanent.
Applications for these cables often involve portable equipment such as power tools or temporary installations such as worksite lighting. These cables have EPDM thermoset rubber conductor insulation material and a black CPE thermoset rubber jacket that provides excellent resistance to abrasion, hot surface contact, harsh conditions, and extreme temperatures.
The new Helukabel SOOW and SJOOW portable cord is cut to length in 1-foot increments with a 20 ft. minimum, starting at $0.33 / ft.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information and the most current pricing on products contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo