January 12, 2022 – AutomationDirect has added new current, rate, process, and temperature meters to their Trumeter ADM series of graphical panel meters.
These panel meters feature a programmable 40-segment curved bar graph display that provides an instant visual representation of an analog meter. In addition, they have a large 4-digit readout, dynamic backlight color, customizable messages, and alarms to alert operators when a parameter is out of range.
The updated free configuration software includes ten alarm points, a 20-point non-linear conversion table, and better scaling. These panel meters come with a 3-year warranty and are UL listed, CE marked, and RoHS compliant.
In addition to the graphical panel meters, AutomationDirect has added a new line of low-cost Trumeter hour meters and counters. Available in electromechanical and battery-powered LCD units, they provide reliable counting and run hours tracking for any application. Optional gaskets are available to allow for NEMA 4/4X rating when mounted in a suitable enclosure.
Trumeter graphical panel meters start at $70.00, and the hour meters and counters start at $18.50
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo