February 5, 2025 – AutomationDirect has added WAGO splicing connectors to their selection of wiring solutions. The 221 series LEVER-NUTS® are equipped with WAGO’s CAGE CLAMP® spring technology, allowing quick and easy connection of all conductor types of different cross sections using two-, three-, and five-wire connectors without soldering or using tools.
The 221 series connectors accommodate solid, stranded, and fine-stranded conductors in two variants from 12-24 AWG and 10-20 AWG. The 221 series inline splicing connector includes all the trusted advantages of the 221 series but in a slim design.
The 2773 series’ PUSHWIRE® technology allows solid, stranded, ferruled, and fine-stranded conductors to be terminated by simply pushing them in, with no operating tool needed.
The New WAGO 2773 series splicing connectors start at $8.00 / 60pk., the 221 series LEVER-NUTS splicing connectors start at $14.00 / 25pk., and the inline 221 series splicing connector is priced at $22.00 / 60pk.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information and the most current pricing on products contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo