January 18, 2023 – AutomationDirect has extended its line of WEG CFW500 high-performance AC drives to include more horsepower options. With this addition, the high-performance horsepower ratings have been expanded all the way up to 150hp.
Also added are new higher current high-performance 10hp drives as well as 10hp washdown rated IP66/NEMA 4X models. A full range of supporting accessories is also included with this launch.
The new WEG CFW500 drives start at $826.00. All WEG CFW500 VFDs and accessories come with a one-year warranty.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo