September 27, 2023 – AutomationDirect has added the Endress+Hauser Micropilot FMR10 series pulsed radar liquid level sensor to their growing lineup of liquid level sensors. This new sensor is a downward facing, non-contact sensor that emits electromagnetic pulses and determines the level based on the time it takes for the pulses to be reflected back to the sensor. Radar sensors are more accurate than ultrasonic sensors and are less affected by environmental conditions such as temperature, humidity, and dust than ultrasonic sensors.
The Micropilot level sensor is configurable via Bluetooth® interface using the SmartBlue mobile app, which includes a linearization function that converts measured values to length, weight, flow, or volume. The mobile app can also display and record process envelope curves, which provide valuable diagnostic feedback for signal strength, range resolution, and interference.
The Endress+Hauser Micropilot FMR10 series pulsed radar level sensor is CSA approved, CE marked, and RoHS compliant. It offers a 1-year warranty and is priced at $720.00.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo