NewsPress ReleasesPress Releases

SSP Magnetic Locking RFID Non-Contact Safety Switches from AutomationDirect

SSP magnetic locking RFID non-contact safety switches

October 4, 2023 – AutomationDirect has added SSP magnetic locking RFID non-contact safety switches to their portfolio of safety products.  The SSP safety switches monitor and lock machine guards, doors, windows, or other machinery.

These safety switches combine both magnetic locking and RFID technology to provide tamper-proof protection using coded actuators. Contact is not required between the switch and actuator, which allows for a degree of misalignment.

Available in master-coded and reteachable-coded models, these switches feature diagnostic LEDS, a Bluetooth interface, and are the perfect size for mounting on SureFrame T-slotted rails.

The new SSP magnetic locking RFID non-contact safety switches come with a 1-year warranty and start at $349.00.

About AutomationDirect:

In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit https://www.automationdirect.com/

Editorial Contact:         Tina Gable

Phone:                         678-455-1845

Email:                          tgable@automationdirect.com

Download:                   High Resolution Photo