![Metal Work Series 70 Valves](https://library.automationdirect.com/wp-content/uploads/2024/05/metal-work-solenoid-valves-launch.jpg)
May 8, 2024 – AutomationDirect has added Metal Work Series 70 valves to their Valves and Pneumatic Components categories. Metal Work is a trusted name in pneumatics and several new valve types are available, including toggle and axial lever manual valves, push-pull manual valves, mechanically operated air valves (mechanical limit switch valves), pushbutton air valves, air pilot valves, and solenoid valves.
Configuration and port sizes include 3-port, 3-way, 2-position, and 5-port, 4-way, 2- or 3-position valves. Coils are sold separately for solenoid valves, allowing for a choice of voltages ranging from 12 VDC to 220 VAC.
Solenoid valves come in internally and externally piloted versions. Externally piloted valves allow a more comprehensive pressure range and control pressures down to full vacuum.
The new Metal Work Series 70 valves have a 1-year warranty and start at $23.00.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo