May 22, 2024 – AutomationDirect has added new discrete and relay I/O expansion modules to the Productivity PLC family. For the Productivity1000 PLC series, a 4-channel, high current relay output module is now available. This module provides up to 7A/point for both DC and AC control circuits and features four Form C (normally open/normally closed) contacts.
For the Productivity2000 PLC series, a 6-channel, high current (7A/point) relay output module is available. A 16-point low voltage discrete input module and a 16-point low voltage discrete output module have also been added. These modules work with devices that utilize transistor-transistor-logic (TTL) and voltage levels ranging from 3.3 to 5 VDC.
The new Productivity1000 high current relay module is priced at $73.00. The Productivity2000 high current relay module is $107.00 and the new TTL discrete I/O modules start at $98.00. All modules come with a 45-day money-back guarantee and a 2-year warranty.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo