NewsPress ReleasesPress Releases

Metrol Precision Limit Switches from AutomationDirect

Metrol limit switches

September 25, 2024 – AutomationDirect has added a variety of new Metrol limit switches to their growing lineup of precision limit switches. These ultra-precise mechanical limit switches have a repeatability down to 0.5 microns (µm) and are some of the smallest switches/sensors available. Their tiny size allows them to be mounted in extremely tight locations.

The additional offering includes precision touch limit switches with a 1-micron repeat accuracy, 90-degree straight touch limit switches with a 6mm smooth barrel, mini stopper precision limit switches in 8, 10, and 13mm flat head styles, and high precision tool setter limit switches with threaded M4 mounting holes or downward installation options. Non-LED limit switch models are also available for a reduced price.

The new Metrol precision limit switches offer a 1-year warranty and start at $36.00.

About AutomationDirect:

In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information and the most current pricing on products contact them at 800-633-0405 or visit https://www.automationdirect.com/

Editorial Contact          Tina Gable

Phone:                          678-455-1845

Email:                          tgable@automationdirect.com

Download:                    High Resolution Photo