NewsPress ReleasesPress Releases

CITO Modular Process Valves & Manifolds from AutomationDirect

CITO StackFlow series of modular process valves

October 23, 2024 – AutomationDirect has added the CITO StackFlow series of modular process valves.  This system of high-flow, robust components can stack together to form a valve bank assembly. Each module includes common inlets at each end and an outlet discharge at the bottom.

Manual and solenoid valves are available, as well as distribution blocks that can all be included in the same assembly. Port adapters are sold separately, allowing multiple threaded connection options to the inlet or outlet port. Flow control outlet port adapters allow fine-tuning fluid flow out of the discharge.

End caps can be placed at one of the inlets and act as a blanking plate or include a temperature or pressure gauge. The new manifolds are rugged general-purpose models with 4 to 8 stations and come with a blue or red anodized finish. Also available are standalone check valves, flow indicators, and numerous modular process valve accessories.

The new CITO modular process and manifold products are proudly made in the USA, have a standard 1-year warranty, and start at $29.00.

About AutomationDirect:

In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information and the most current pricing on products contact them at 800-633-0405 or visit https://www.automationdirect.com/

Editorial Contact          Tina Gable

Phone:                         678-455-1845

Email:                          tgable@automationdirect.com

Download:                   High Resolution Photo