![Murrplastik frames and grommets](https://library.automationdirect.com/wp-content/uploads/2025/02/murrplastik-cable-entry-launch.jpg)
February 5, 2025 – AutomationDirect has added more Murrplastik frames and grommets to their current offering of cable entry systems. Cable entry frames used in conjunction with the required grommets provide easy cable installation through an enclosure and strain relief while maintaining environmental ratings.
This expansion adds more frame sizes to our existing KDL/D and KDL/D-Mono series, a blank large BTG/XL grommet to the KDT/X series, and the new KDL/D-R and KDP/Z series, which provides more solid- and split-frame options. The KDP/Z series features a built-in sealing membrane that does not require separate grommets to be purchased.
The new Murrplastik KDP/Z series frames have a high IP65, IP66, IP67, IP69K protection rating (depending on model) and start at $63.00; KDL/D, KDL/D-R, and KDL/D-Mono series frames start at $29.00, and KDT/X and BTG/XL large grommets start at $15.00.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information and the most current pricing on products contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo