NewsPress ReleasesPress Releases

Wenglor OPT25 Series Laser Distance Measurement Sensors from AutomationDirect

Wenglor OPT25 series laser measurement sensors

March 26, 2025 – AutomationDirect has added Wenglor OPT25 series laser measurement sensors that offer best-in-class distance sensing for ranges within 1 meter. These sensors are IO-Link v1.1 compatible, employ a Class 1 red or Class 2 blue laser, use triangulation to measure distances with extreme accuracy, and can reliably detect tiny objects with a reproducibility up to 0.8μm.

Powered by Wenglor’s proprietary TripleA technology, the OPT25 series ensures precise distance readings regardless of object material, color, or shape, even in demanding environments with fluctuating light and temperature conditions. They can even detect flat objects directly in front of a background. Signal splitters are also offered that allow two sensors to make automatic thickness measurements.

Blue laser light models provide enhanced performance for red-hot or organic surfaces, polished metals, shiny plastics, or dark paints. The shorter wavelength blue laser light does not penetrate as deeply into the surface, resulting in high accuracy. Sensor configuration methods vary by model, with options including a teach-in button, an easy-to-read OLED display, or the intuitive Wenglor weCon Bluetooth app.

The new Wenglor laser measurement sensors are UL Listed, CE and UKCA marked, and RoHS compliant. They offer a 1-year warranty and start at $802.00.

About AutomationDirect:

In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information and the most current pricing on products contact them at 800-633-0405 or visit https://www.automationdirect.com/

Editorial Contact          Tina Gable

Phone:                         678-455-1845

Email:                          tgable@automationdirect.com

Download:                   High Resolution Photo