April 30, 2025 – AutomationDirect has added Lika draw wire linear measurement devices, also known as string encoders or string potentiometers, which use a steel cable wrapped on a spring-loaded reel to measure distance. The reel is connected to a rotary encoder or potentiometer that can provide very accurate feedback on how far the steel cable has been extended. Lika draw wire encoders provide encoder (quadrature) or 0-10V or 4-20mA analog outputs and are available in pull lengths from 2 to 10 meters.
They are a good solution when the operational space is constricted or the environmental conditions are severe. The body of the encoder can be mounted in a safe place, easily accessible, and adequately protected, while the measuring wire requires minimum space and can be subjected to harsher conditions. They can also replace traditional encoders in some cases.
Typical applications include linear measuring, vertical lift measurement, cylinder stroke measurement, or any application where accurate, inexpensive, and easy-to-install measurement of a linear distance is required.
The new Lika draw wire encoders start at $249.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information and the most current pricing on products contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo