NewsPress ReleasesPress Releases

Balluff EtherNet/IP IO-Link Master Modules, Hubs, and Analog Converter from AutomationDirect

Balluff EtherNet/IP IO-Link master module

May 14, 2025 – AutomationDirect has added Balluff EtherNet/IP IO-Link master modules that provide EtherNet/IP communication for IO-Link systems, with a REST API and/or MQTT support depending on model. They are available in a rugged IP67 die-cast zinc nickel-plated housing for harsher environments or in a weld-proof potted plastic format. Select models include built-in screen interface for easy IP, subnet mask, and gateway configuration.

Balluff IO-Link hubs allow several sensors and actuators to be easily connected to an IO-Link master via a standard sensor cable and are housed in die-cast zinc nickel-plated housings to withstand extreme conditions. These hubs transmit standard field I/O signals, including analog and temperature data. Both masters and hubs are machine mountable and do not require enclosures.

Also available is a Balluff IO-Link analog converter, which provides a low-cost solution to convert various analog I/O signals into a single I/O-Link connection.

The Balluff EtherNet/IP IO-Link master modules start at $549.00, the new IO-Link hubs start at $291.00, and the IO-Link analog converter is priced at $249.00.

About AutomationDirect:

In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information and the most current pricing on products contact them at 800-633-0405 or visit https://www.automationdirect.com/

Editorial Contact          Tina Gable

Phone:                         678-455-1845

Email:                          tgable@automationdirect.com

Download:                   High Resolution Photo