June 7th, 2023 – AutomationDirect has added Bryant pin and sleeve mechanical interlocks to their growing lineup of motor disconnects and controllers. These interlocks use pin and sleeve technology to conveniently connect and disconnect mobile equipment safely. By using matching Bryant pin and sleeve connectors with keyways, these interlocks safeguard against connecting devices of different amperage and voltage ratings together. In addition, the interlock’s switch cannot be turned ON until the plug is completely engaged and the plug cannot be removed from the interlock until the switch has been turned to the OFF position.
These Bryant interlocks are suitable for use as manual motor controllers and their handles satisfy OSHA lockout/tagout requirements. Pin and sleeve devices conform to IEC 60309-1 and IEC 60309-2 international regulations, resulting in easy-to-use and standardized configurations.
New Bryant pin and sleeve mechanical interlocks are UL Listed, CE marked, and RoHS compliant. They offer a 1-year warranty and start at $513.00.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo