June 19, 2024 – AutomationDirect has added CCEA VEGA series recessed industrial LED light bars to expand their offering of industrial LED fixtures. Specifically designed for medium and large CNC equipment, these compact fixtures feature a rugged, ultra-slim anodized aluminum housing that is highly resistant to dust and liquids and allows mounting outside the machine’s working area. These 24 VDC rated LED lights provide intense, uniform lighting, with up to 3,300 lumen output and a 120° beam angle.
CCEA VEGA series LED light bars are offered in 13.62in (346mm), 18.35in (466mm), and 27.80in (706mm) lengths. They are UL recognized, CE marked, and start at $174.00.

About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information and the most current pricing on products contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo