May 28, 2025 – AutomationDirect has added CHANNELLOCK tools, which are designed with strength and durability in mind. CHANNELLOCK tools are made in the USA with high-carbon USA steel. The CHANNELLOCK straight jaw pliers feature undercut tongue-and-groove channels to prevent slipping, and Griplock jaw tongue-and-groove pliers have an offset head for greater leverage with patented SAFE-T-STOP® technology to prevent pinching. CHANNELLOCK long nose pliers, with a crosshatch tooth pattern and narrow nose profile, and slip joint pliers, with a serrated jaw and an added wire cutting shear, are perfect for soft wire. High-leverage diagonal/curved cutting pliers, with precision-machined knife and anvil-style cutting edges, ensure perfect mating for superior performance and longevity. Assorted pliers sets as well as technicians’ pliers sets are available.
New CHANNELLOCK multi-purpose wiring tools feature models that can perform a variety of tasks, including wire stripping, wire cutting, deburring, reaming, crimping, or bolt cutting.
CHANNELLOCK adjustable wrenches are made of rugged chrome vanadium steel and feature non-protruding jaws for accessing hard-to-reach areas. Measurement scales are laser-engraved for sizing nuts, pipe, and tube diameters while its four-thread knurl adjuster boosts accuracy. Models with extra-wide jaws are also available to accommodate larger nuts and bolts.
The new CHANNELLOCK pliers start at $14.00 (526), multi-purpose wiring tools start at $16.00 (958), adjustable wrenches start at $18.00 (804), and tool sets start at $45.00 (WS-2).
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information and the most current pricing on products contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo