April 27, 2022 – AutomationDirect has released the new CLICK PLC programming software version 3.30, which allows any CLICK PLUS CPU to be configured as a 3-axis PTO/PWM motion controller. 100kHz high-speed inputs and outputs are offered with any DC option slot I/O module placed in slot 0 of the CPU.
With this module, CLICK PLUS PLCs can easily perform velocity moves, homing commands, or interpolated positioning. The easy-to-use configuration GUI built into the software and the three new motion instructions (Velocity Move, Position Move, and Home) make it a cinch to control simple motion applications.
CLICK PLUS PLCs are the next generation of the popular CLICK PLC series, maintaining the simplicity of the original CLICK but with advanced capabilities, including Wi-Fi communication, MQTT support, data logging, and now motion control.
CLICK PLUS CPUs start at $93 with FREE software, high-speed I/O capable option slot modules start at $56, and both come with a two-year warranty.
Learn more by visiting: http://www.automationdirect.com/click-plus-software
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo