May 5, 2021 – AutomationDirect has added Datalogic Safety Laser Scanners to its lineup of safety products.
Safety laser scanners offer an ingenious, cost-effective way to protect an entire area. This can be a static application such as a robot cell or the area surrounding a moving device such as an AGV.
They are ideal for providing safe access to potentially dangerous locations or areas.
These laser area scanners are configurable and feature a 275-degree viewing window that allows for several user-defined zones of protection. I/O and dust filtering are other options configurable through the unit’s GUI.
Mounting brackets and replacement windows are available.
These new Datalogic Safety Laser Scanners start at $1,992.00 and have a 3-year warranty.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Downlaod: High Resolution Photo