July 24, 2024 – AutomationDirect has added the new SQ series table lifting systems from Ergoswiss. These lifting systems use electrically driven columns that allow the operator to reposition the height of a worktable, conveyor, etc., to meet their specific requirements. In doing so, the operator can perform their tasks in a more comfortable working posture, helping to reduce work-related injuries.
These systems are all electric (no hydraulic mess or manual hand cranks) and each lifting column features an enclosed motor and screw drive to perform the needed height adjustments. Simply raise or lower equipment with simple pushbutton controls and save the preferred position in the controller using the 3 memory settings. Up to 4 lifting columns can be connected to one control box for up to a 1320lb weight capacity or sync two control boxes and control up to 8 lifting columns.
Lifting columns offer stroke lengths of 300mm [11.8”] or 400mm [15.7”] and are sold individually or in convenient kits with everything needed to install a complete lifting system. Ergoswiss lifting systems work well with SureFrame 15 series and 40 series T-slotted rails and include a tilt sensor for added safety that will stop operation if a tilt of more than 2.5 degrees is detected.
The new Ergoswiss lifting system kits start at $2,100.00 or purchase components separately, starting at $20.00. All lifting system components and kits come with a 45-day money-back guarantee and a 1-year warranty.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information and the most current pricing on products contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo