June 22, 2022 – AutomationDirect has added a new line of enclosure filter fans to their inventory of thermal management devices. The Fandis Virdis series filter fans provide a low-cost thermal management solution for applications where the surrounding cooler air can be used to reduce the internal temperature of an enclosure.
The Virdis series fans are available in both NEMA 12 and 3R models. NEMA 12 rated models are for indoor use, and NEMA 3R versions are specifically designed to preserve the integrity of components housed within an electrical enclosure located outdoors.
Fandis filter fans are available in various voltages and dimensions, with roof mount units offered for limited space applications.
The Fandis Virdis series also includes vents and grilles that work with the fans to draw filtered cooler ambient air into the enclosure. These vents and grilles come in various sizes and materials.
The new Fandis Virdis series filter fans start at $67.00 with vents and grills starting at $13.25.
About AutomationDirect
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo