August 28, 2024 – AutomationDirect has added Gladiator GR series DIN rail or panel mounted quad-port power receptacles. These receptacles provide convenient power outlets and are commonly used in electrical enclosures to temporarily power laptop computers and test equipment. The GR-REC4 consists of two NEMA 5-15R duplex receptacles, while the GR-REC4-GFCI includes one standard NEMA 5-15R duplex receptacle and one GFCI duplex receptacle that provides protection for all four circuits.
The new Gladiator receptacles are UL recognized, CE marked, and RoHS compliant. They offer a 2-year warranty and start at $48.00.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information and the most current pricing on products contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo