The new StrideLinx Premium Branding License from AutomationDirect allows the creation of a custom company IoT platform with a user-specified domain name, the company logo on the login screen, and customized support and contact information. The Premium Branding license is $1,850.00 (one-time charge).
StrideLinx provides secure access over the “industrial internet” to remotely connect, monitor, and troubleshoot multiple field devices. StrideLinx easily and affordably cloud enables any Ethernet-ready device.
The StrideLinx platform consists of three types of VPN routers and two antenna sets (Wifi and cellular). 5GB monthly data bandwidth is included free and subscription options include additional bandwidth (up to 50GB) and cloud data logging. The StrideLinx platform allows unlimited users, and unlimited concurrent client and mobile connections.
Subscription options provide added services to the StrideLinx remote access solution. Subscriptions are not needed for the basic function of the VPN but can be added to enhance the value of the platform. Cloud data logging, for example, allows system data to be saved within the platform for a convenient, web-based live or historical record of system performance available whenever needed. Purchase your StrideLinx Premium Branding license for use on the “industrial internet” today!
For more information visit www.automationdirect.com/Stride-StrideLinx.
Click here to view more press releases from AutomationDirect.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com