September 11, 2024 – AutomationDirect has added Master Appliance heat guns, which are quality heating tools used extensively across various industries for tasks such as shrinking tubing, activating adhesives, bending plastics, thawing frozen pipes, circuit board manufacturing, and so much more. These heat guns deliver high temperatures quickly and efficiently and include various models to fit most applications.
D-series fixed-temperature heat guns are heavy-duty industrial tools that provide up to a 1200°F heat source with a high 27 CFM and 3400 FPM airflow. Varitemp® heat guns include an adjustable 130°F to 1200°F temperature dial, with a high 27 CFM and 3400 FPM airflow. The Master-Mite heat gun is a 650°F continuous-duty bench-top heating system with a quiet motor that performs tasks without excess air flow. The EC-Mini heat gun is a professional grade 640°F heat tool with a small footprint that is lightweight, portable, and a versatile heat source for many tasks and projects. Master-Mite and EC-Mini models include a height-adjustable stand for hands-free use.
Master Appliance D-series heat guns start at $180.00, Varitemp heat guns start at $240.00, the Master-Mite heat gun is priced at $140.00, and the EC-Mini heat gun is priced at $31.50.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information and the most current pricing on products contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo