December 11, 2024 – AutomationDirect has added Murrelektronik Premium EtherCAT IO-Link master modules to their IO-Link product lineup. IO-Link masters provide standardized, point-to-point connections between smart devices and controllers. IO-Link functions similarly to traditional field I/O but adds the capability to collect diagnostic and operational data from IO-Link capable devices, helping pinpoint potential problems or improvements. Typical IO-Link systems consist of one IO-Link master (the interface between IO-Link and higher-level systems) and at least one IO-Link device.
The new Murrelektronik master module adds EtherCAT capability for systems that utilize this powerful protocol. Premium master modules also include MQTT and OPC UA communication for high-level data collection and cloud/IIoT networking.
Murrelektronik IO-Link hubs allow several sensors and actuators to connect easily to an IO-Link master via a standard sensor cable. These hubs transmit standard field I/O signals, and several new models have been added, including more discrete I/O modules and modules that support analog/temperature inputs.
The Murrelektonik Premium EtherCAT IO-Link master module is priced at $399 and the new IO-Link hubs start at $215.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information and the most current pricing on products contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo