May 12, 2021 – AutomationDirect has added more choices to their offering of Murrplastik cable entry systems.
The addition of the KDL/D MONO series cable entry system provides the same benefits as the existing KDL/D series in a round frame form. This series allows a cable to be installed through an enclosure or other bulkhead surfaces, with the added benefit that pre-made, terminated cables can be installed without disassembling the connectors.
The newly added KDP/X cable entry system allows for a high density of non-terminated cables to be installed through a small area of an enclosure or other bulkhead surfaces.
The KDL/D MONO series is available in 3 frame sizes and starts at $36.00. The KDL/D series is available in 4 frame sizes and starts at $16.00. The KDP/X is available in one frame size, with bolt-in or snap-on mounting, and starts at $29.00.
The new Murrplastik cable entry systems are easily assembled and have a 2-year warranty.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo