November 15, 2023 – AutomationDirect has added additional CSmicro and new CSlaser series infrared pyrometers to their growing lineup of temperature sensors. Infrared pyrometers use non-contact sensing to determine the surface temperature of an object based on its emitted infrared radiation.
Optris CSmicro LTH, 3ML/3MH, and 2MH series miniature infrared pyrometers feature a rugged stainless steel construction and provide additional temperature ranges up to 1600°C (2912°F) with new wavelengths that can measure temperatures through glass or can measure metal and shiny surfaces.
The new Optris CSlaser LT and 2ML/2MH series pyrometers feature an innovative double laser aiming system that instantly indicates the size of the area and the location on a target where the temperature is sensed. The CSLaser pyrometers use Q7525-1 (4/c, 22 AWG) or Q8180-1 (6/c, 24AWG) cut-to-length cables (ordered separately) which can be tailored to any desired length for installation.
The new Optrics CSmicro series infrared pyrometers start at $370.00 and the new Optrics CSlaser series infrared pyrometers start at $635.00.
Optris infrared pyrometers are CE marked, RoHS compliant, and have a 2-year warranty.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo