May 14, 2025 – AutomationDirect has added Pfannenberg DTT 6000 series top-mounted air conditioners which are 100% condensate safe, provide up to 14,000 BTU/H, and are ideal for space-saving installation on the top of a NEMA 12 control enclosure. Pfannenberg’s DTS series 3000 air conditioners are made in the USA, offer cooling capacities up to 25,000 BTU/H, and can be used with NEMA/UL Type 3R, 4, 4X, and 12 enclosures. They offer several frame sizes, filter-free operation, and feature compressor and fan motors outfitted with integral temperature switches.
Pfannenberg air-to-water heat exchangers are ideal for applications where a tempered water source is readily available and in any environment where ambient air temperature is high and the atmosphere is corrosive. Air-to-water heat exchangers have a high cooling capacity, are extremely energy efficient, and require less maintenance once established.
Premium quick filter rolls from Pfannenberg provide a low-cost, single-use filter option. These premium quick filters are affixed externally, acting as the first line of defense for critical equipment and eliminating the need for tools and maintenance downtime when a filter change is needed. 60 filter sheets per roll allow for more than a year’s worth of fast weekly changes.
The new Pfannenberg air-to-water heat exchangers start at $1,536.00, air conditioners start at $2,698.50, and PQF rolls start at $119.00.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information and the most current pricing on products contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo