December 7, 2022 – AutomationDirect has added more low-cost ProSense float level switches. The new offering includes the FLS-VM-800 float switch which has a 3/4″ PVC pipe fitting for use in HVAC condensate lines, and the FLS-VD series that includes a 3/4″ MNPT connection for mounting to most standard 3/4” bungs in 55-gallon drums.
A selection of top- and side-mount float switches, in medium and large sizes, has also been added with various material constructions for compatibility with a variety of liquid types, temperature ranges, and system pressures.
The new ProSense float level switches are UL recognized, CE marked, RoHS compliant, come with a 1-year warranty, and start at $17.25.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo