September 11, 2024 – AutomationDirect has added more options to the ReeR MOSAIC safety controller family. The MOSAIC-M1S-USBC has all the features of the enhanced MOSAIC-M1S master controller module, including embedded digital inputs, OSSD outputs, and expansion capabilities, but also offers a USB-C programming port.
The new ReeR MOSAIC MZERO controllers are simple standalone safety controllers that have plenty of fixed I/O but do not support expansion I/O. They are ideal for small systems with fewer safety devices. Also available is a proprietary memory card for use with these controllers.
All ReeR safety controllers come with a standard 1-year warranty and start at $463.00.
Learn more by visiting: https://www.automationdirect.com/safety-controller
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information and the most current pricing on products contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo