July 17, 2024 – AutomationDirect has added new Saginaw Enviro-Therm® air-to-air heat exchangers that use the enclosure’s ambient air and either heat pipes or aluminum plate to transfer heat from inside the enclosure to the external environment. Since the ambient air is the cooling medium, the need for refrigerant is eliminated.
Features include corrosion-resistant internal components, a filter-less design for maximum cooling and reduced clogging, simple installation using threaded mounting studs, a programmable digital controller, and many other great features.
The new Saginaw Enviro-Therm® air-to-air heat exchangers are cULus recognized Type 3R and 12 and start at $1,119.00.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information and the most current pricing on products contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo