June 14, 2023 – AutomationDirect has added the 10 (1 inch), 15 (1.5 inches), and 40 (40mm) series of SureFrame rails, in standard and light weights. These new rails are offered with a UV-resistant black anodized finish, which provides a new aesthetic option in addition to the standard clear anodized finish that is available for all series and weights of SureFrame T-slotted rails.
SureFrame rails are used to build sturdy, custom-made structural frames and are warranted from manufacturer defects for one year from the date of purchase.
The new black anodized SureFrame rails can be ordered in cut-to-length sections starting at $0.37/inch.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo