May 1, 2024 – AutomationDirect has added more WEG Electric S series premium efficiency motors to their expanding portfolio of AC motors. This addition includes several general-purpose 3-phase motors from 1-1/2 to 20hp and 3-phase brake motors from 3 to 20hp.
The new rolled steel motors are available with speeds of 1200, 1800, and 3600 rpm, while brake motors are rated for 1800rpm. The 230/460 VAC-rated brake motors come with a spring set, solenoid actuated AC brake, and manual release brake lever.
The new WEG rolled steel and brake motor additions start at $518.00 and have a 3-year warranty.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo