April 22, 2021 – AutomationDirect has added a new line of laser sensors. Wenglor dark and shiny object detection photoelectric sensors use blue light technology to detect objects other photoelectric sensors cannot see or see objects that get detected multiple times erroneously.
They come in either 50x20x50mm or 32x12x16mm body sizes with an M12 or M8 quick-disconnect.
These sensors can detect dark and shiny objects up to 400mm away and are IO-Link V1.1 compatible.
Also added are four new models to the Wenglor performance line and five laser sensors to the discrete distance detection group.
These new Wenglor sensors start at $91.00 and have a 1-year warranty.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.
Editorial Contact: Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo