October 9, 2024 – AutomationDirect has added more top-of-the-line Wera tool options to their continuously growing Tool and Test Equipment lineup. New tool sets include maintenance sets, a Joker self-setting/self-adjusting wrench set, a Tool-Check PLUS socket/driver bit set, and Kraftform Kompakt multi-bit screwdriver sets.
Screwdriver additions include Kraftform Micro precision screwdriver sets, Kraftform Kompakt multi-bit screwdriver sets and multi-bit handles. More torque screwdrivers including Kraftform Safe-Torque compact adjustable torque screwdrivers and an adjustable torque screwdriver with pistol handle.
We’ve also added more options for Hex-Plus hex and torx L-key wrenches as well as a selection of Joker self-setting/self-adjusting ratcheting wrenches in various sizes.
The new Wera tool sets start at $42.00, multi-bit screwdrivers start at $22.00, torque screwdrivers start at $90.00, Hex-Plus L-keys start at $12.00, and Joker adjustable wrenches start at $38.00.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency, and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information and the most current pricing on products contact them at 800-633-0405 or visit https://www.automationdirect.com/
Editorial Contact Tina Gable
Phone: 678-455-1845
Email: tgable@automationdirect.com
Download: High Resolution Photo