AutomationDirect announces the release of a new White Paper, “Basic Pneumatic Circuits”, which discusses common pneumatic circuits that can be used alone or as building blocks in larger pneumatics systems.
This white paper examines pneumatic design best practices and presents four basic pneumatic circuits commonly used in machine automation. The four basic pneumatic circuits examined in the paper include the air preparation subsystem, double-acting cylinder circuits, continuous cycling cylinder circuits and two-hand control circuits.
As discussed, the first basic pneumatic circuit needed provides consistent plant air pressure and flow required for pneumatic devices to operate consistently and reliably. Common in many machines, a pneumatic circuit consisting of a 4-way solenoid valve operating to automatically extend and retract a double-acting air cylinder is detailed. A circuit example of how pneumatic components are combined in a well-thought-out design to continuously cycle a cylinder is discussed, as is the pneumatic circuit for a two-hand safety control system for a press application.
There have been many innovations over the years, and the basic pneumatic components such as valves, solenoids, cylinders, hoses and fittings are well developed and mature. These devices can be combined in many ways to provide simple and reliable machine control.
The “Basic Pneumatic Circuits” White Paper can be downloaded here.
About AutomationDirect:
In business since 1994, AutomationDirect is a distributor offering thousands of industrial automation products for electrical control systems, including PLCs, operator interfaces, AC drives, motors, stepper systems, sensors, motor controls, enclosures and more. Their prices are typically well below the list price of more traditional automation companies because of their business model and focus on efficiency and the majority of their products are stocked for fast shipping. Plus, get free two-day delivery on orders over $49; some limitations apply. For more information, contact them at 800-633-0405 or visit www.automationdirect.com.
Editorial Contact: Tina Gable
Phone: 678-455-1845 Email:
Email: tgable@automationdirect.com