Sign Up for our Newsletter Here!

Here’s What to Expect:

  • Applications – Industry articles & customer stories
  • Tech Tips – FAQs, discussions & technical info.
  • Videos – How-to and What’s-New videos
  • Product Views – New products, specs, prices
  • Online Features – Newest web features, helpful tips
  • Company News – The latest from AutomationDirect

We promise to keep our emails short and sweet!
Also, we respect your privacy and will never share your address with anyone.

Current Newsletter

Check Out Some of Our Past Newsletters- No Sign Up Necessary!

NewsletterNewsletter

Newsletter Volume 27 Issue 8

Automated Robotic Welding Cuts Production Time by Over 90% A manufacturing company teamed up with a systems integration firm to significantly accelerate an infrastructure project by integrating a robotic welder with precision motion control, intelligent safety systems, and other advanced automation components. Learn more Demystifying Motion Control Anyone who has ever observed a modern factory…
NewsletterNewsletter

Newsletter Volume 27 Issue 7

Beyond Safety Slogans: Cultivating a Workforce Culture to Protect People and Productivity Industrial safety standards have undergone a significant transformation in recent years, primarily driven by the integration of automation and robotics into manufacturing environments. Traditional lockout and tagout procedures have evolved into sophisticated safety systems that incorporate real-time monitoring, predictive analytics, and zone-based safety…
NewsletterNewsletter

Newsletter Volume 27 Issue 6

New Product Giveaway – CHANNELLOCK! Enter your info for a chance to win some of our newest products. This giveaway includes (2) 9.5-in. pliers, (2) 6.5- in. pliers and (2) 6-in. wire strippers. You will also be entered to win 1 of 5 drill bit sets. Contest is open for approximately 3 weeks after the…
NewsletterNewsletter

Newsletter Volume 27 Issue 5

Solving Frequency Signal Conditioner Challenges Frequency signal conditioners—designed to handle high-frequency pulse signals from sensors and convert them into other useful automation signals—are an important industrial automation design component for both new and retrofit applications. High-frequency pulses may be generated from a proximity sensor associated with a spinning sprocket, between digital motion control systems requiring…
NewsletterNewsletter

Newsletter Volume 27 Issue 4

How to Choose a Sensor for the Production Environment Sensors play essential roles in the modern production environment, capturing data on position, speed, proximity, pressure, temperature, level, flow, current, voltage, and more. There is such a wide variety of sensors on the market that finding the right device for your application can seem overwhelming. It…
NewsletterNewsletter

Newsletter Volume 27 Issue 3

Six Tips to Help You Build a Better, Safer Machine Safety is an essential aspect of machine design and operation, protecting personnel, guarding against equipment damage, and maximizing productivity. The purpose of a safety system is to bring a machine to a known safe state as quickly as possible after a safety sensor detects a…
NewsletterNewsletter

Newsletter Volume 27 Issue 2

Unshackling Industrial Data Access Modern consumers are increasingly familiar with tailored experiences, abundant information, and generally getting things “their way.” Those working in the industrial manufacturing and automation sectors, on the other hand, have not always enjoyed such flexibility. Fortunately, hardware and software advancements mean that access to valuable industrial sourced data is easier, more…
NewsletterNewsletter

Newsletter Volume 27 Issue 1

Build Better Machines Faster Using Today’s Enhanced Motion Controllers and PLCs High-performance servo motion is now more affordable and accessible than ever due to integrated controllers, making the technology viable even for applications which could not formerly support the cost or complexity of traditional implementations. Learn more The Master Controller of Motors Everyone knows that…
NewsletterNewsletter

Newsletter Volume 26 Issue 12

Simplified Motion Control High-performance servo motion is now more affordable and accessible than ever due to integrated controllers, making the technology viable even for applications which could not formerly support the cost or complexity of traditional implementations. Learn more Turning Up the Heat on a Balky Boiler Applying commercial off-the-shelf automation products can provide the…
NewsletterNewsletter

Newsletter Volume 26 Issue 11

3-Axis Motion Made Simple in 3 Ways using CLICK PLUS PLCs | White Paper AutomationDirect CLICK PLUS PLCs, when combined with stepper motors, make advanced motion control and edge integration simple for smaller systems. Electric motors provide the motive force for many types of machinery and equipment. Sometimes standard AC and DC motors are operated…
NewsletterNewsletter

Newsletter Volume 26 Issue 10

Early fault detection and simple plug-and-play field replacements In addition to the large amount of process data available cyclically, faults can be identified easily through diagnostic information messages. This includes device faults, such as memory or processor failures, or process faults like empty pipe detection. Comprehensive diagnostics reporting increases overall system reliability and boosts customer…
NewsletterNewsletter

Newsletter Volume 26 Issue 09

Big Rig Custom Shop Accelerates Automation into the Passing Lane “Less is more” and “function over form” are phrases often associated with the design of objects—anything from office supplies up to buildings or larger—to promote a concept of simplicity, clarity, and essential purpose. However, there are plenty of cases where most people would agree that…
NewsletterNewsletter

Newsletter Volume 26 Issue 08

Options for Open Industrial Programming Industrial automation designers now have a variety of ways to incorporate an open programming approach for their projects. Although industrial-grade digital technologies have been available for over five decades, much of that time the hardware and software has been specialized and even proprietary. This is at odds with a large…
NewsletterNewsletter

Newsletter Volume 26 Issue 07

Starting Digital Transformation from the Edge While many operations personnel at production and manufacturing companies are aware that their automated equipment can be a source of valuable data for analytics and other purposes, far fewer companies are positioned to create the required IIoT infrastructure to access this information. Learn more PLCs Can Deliver Advanced Motion Control…
NewsletterNewsletter

Newsletter Volume 26 Issue 06

The Evolution of Controls from Relay Logic to IEC Programming In this video, Doug Bell from Interconnecting Automation discusses the evolution of machine control from relays to the first PLC with ladder logic and now IEC programming. Watch the video Installing a Rock-Solid Automation Retrofit This electrical contractor relied on AutomationDirect PLC and HMI hardware and…
NewsletterNewsletter

Newsletter Volume 26 Issue 05

From Ethernet to EtherCAT and Beyond Once upon a time (think 1980s), Ethernet was a relatively specialized computer connectivity technology, administrated by experienced gurus under highly-controlled office settings. Since then, technology and performance have advanced incredibly, and much of the world?s population uses wired and wireless (Wi-Fi) Ethernet in their everyday lives. Learn more AutomationDirect Named…